AXIS#.IPEAK

Description

AXIS#.IPEAK returns the drive peak rated current in Arms.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Arms

Range

N/A

Default Value

N/A

Data Type

Float
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
AXIS1.IPEAK

5000h

0ch

Signed32

-

1000:1

Read only

No

AXIS2.IPEAK

5100h

0ch

Signed32

-

1000:1

Read only

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.IPEAK

5014

1396

Unsigned32

Read Only

-

AXIS2.IPEAK

70550

1139

Unsigned32

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.IPEAK

5014

Float

Read Only

-